EEO#.ZOFFSET

Description

Sets the position within each revolution where the Z pulse will be generated, when the one Z pulse per revolution mode is selected (EEO#.ZMODE 0).

When the primary feedback position (within a revolution) equals this value, an index pulse will output.

When using multi-turn or single turn absolute feedback devices, the Z pulse generated by the EEO will always be aligned with the same mechanical position as the primary feedback position. When using an incremental feedback deviceClosed A process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position, the origin of the primary feedback is not at the same mechanical position each time the drive powers up.

Examples

Code

To set the Z pulse to be generated at an offset of 90 degrees (1/4 turn) expressed in counts:

-->EEO1.ZOFFSET 1073741824 [Counts]

Context

For more information see Output - Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000  

General Information

Type Read/Write
Units Depends on units used by feedback source selected by EEO#.SOURCE
Range Depends on units. See Position Range for details.
Default Value 0
Data Type Integer
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Fieldbus Information

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable

EEO1.ZOFFSET

4600h

07h

Unsigned32

-

-

Read/Write

No

EEO3.ZOFFSET

4603h

07h

Unsigned32

-

-

Read/Write

No

EEO4.ZOFFSET

4606h

07h

Unsigned32

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

EEO1.ZOFFSET

32030

7D1E

Unsigned32

Read/Write

-

EEO3.ZOFFSET

32032

7D20

Unsigned32

Read/Write

-

EEO4.ZOFFSET

32033

7D21

Unsigned32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

EEO1.ZOFFSET

32030

Unsigned32

Read/Write

-

EEO3.ZOFFSET

32032

Unsigned32

Read/Write

-

EEO4.ZOFFSET

32033

Unsigned32

Read/Write

-